Hello Everybody,
We have an EVMK2HX Multicore DSP Evalboard with 66AK2H. BMC version is 1.0.2.7, board version is Rev 4.0, EVM Superset is K2KH-EVM,
EVM Subset is XTCIEVMK2X
It (by the Userguide) should be able to boot via Ethernet using BOOTP protocol.
In despite of this the function doesn't work.
I've set the onboard DIP switches to #5, that is the bootmode the booting via Ethernet. At the BMC> prompt it's confirmed.
After power on I watch the network traffic by the Wireshark, but I can't see any network traffic.
The network and network settings are correct, because if I load a U-Boot from flash, I can boot up the Linux kernel and the filesystem from Ethernet.
I've met a similar post on this forum, so this problem has come up. I'm interesting there is a solution for this yet ??
Thanks in advance
Gabor