Hi all,
The device I used is 66AK2H14 and I load the GEL file from C:\ti\ccsv6\ccs_base\emulation\boards\xtcievmk2x\gel\xtcievmk2x.gel.
In this GEL file, there is a function to check the PACLKSEL.
Here, PASSCLKSEL_MASK equals to (1 << 17).
But in the DEVSTAT, the bit 17 is not related to PASSCLKSEL.
So it's the problem confused me.
Could anyone explain this?
And whether is the PACLKSEL pin high or low can set the PA to use the PACLK rather than SYSCLK? It's not clear in the 66AK2H14 data manual.
Regards,
Feng