I have a EVMK2H rev 4.0 and I am trying to load a "hello wolrd" application through U-boot.
I did:
1) set ipaddr and serverip variables
2) created bin file using objcopy
3) transfer via tftp
4) run it using "go <address>"
It hangs on the message "starting application at <address>"
my questions:
- want is a valid address (or range of addresses) for this board ? I've tryed multiple among 0x80008000, 0x88000000 without result
- should I be using "bootcmd" instead of "go" ?
- do I need to set or modify any environment variable?
Regards