Hi,
I'm using 6678 device that has three PKTDMA and one of them is placed in QMSS. I understand that SRIO PKTDMA rx and tx channels are connected to SRIO segmentation contexts (there is no any definition of it in SRIO docs). Something similar must be in Network subsystem. So the questions are:
1) Does rx and tx channels of QMSS internal PKTDMA are connected to each other?
2) What is the mapping of this channels?
3) Can I open tx channel #0 and rx channel #1 to make core-to-core transfers or I must use the same channel numbers?
4) Does the rx and tx channels are some kind of hardware (physical link between data source\dest (SRIO) and DMA engine), while flow is an abstraction over this hardware?
Thanks
Andrey