Hi,
I want to using one aa6k2h12 to encode 1080p @ 60fps and also using this aa6k2h12 to decode 1080p @60fps.The decode and encode functions are not running on the same time.
I have test h264hpvdec on evmk2h borad successfully and using core 0~7.
Also I have test h264hpvenc on evmk2h borad successfully with using core 0~3.
The above two tests are done in seperate using C66x_h264hpvdec_01.01.06.00_ELF and C66x_h264hpvenc_01_00_03_00_ELF demo.
Now I want to merge the encode and decode function into one applications, and encode function will use core 0~7 and decode function will use core 0~3 and the two functions can't be operating simutaniously (sometime just encoding only or sometime just decoding only ).
Questions:
1. Is this scenario correct?(encode and decode have some cores overlaps --core 0~3)?
2. If it is right, is there any demo or example including encode and decode functions ?
3. If the above two are not fulfilled, can you give some suggestions.