Hello All,
How many peripherals (ADCs) can I connect using SPISCS ( chip select ) in TMS320c6678 evm? or How many chip select lines does the said DSP provide in 4 pin operation ?
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
How many peripherals (ADCs) can I connect using SPISCS ( chip select ) in TMS320c6678 evm? or How many chip select lines does the said DSP provide in 4 pin operation ?
Regards
Hi,
See section 7.14 in C6678 Data Manual:
"The C6678 SPI supports two modes, 3-pin and 4-pin. For the 4-pin chip-select mode, the C6678 supports up to two chip selects"
So you should be able to connect up to two slave devices on the SPI.
Best Regards,
Yordan