ti.catalog is not installed in the system. Ensure that the platformproduct or the complete XDCtools productis installed.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ti.catalog is not installed in the system. Ensure that the platformproduct or the complete XDCtools productis installed.
Are you using any SDK for this platform. It appears that you have not setup your CCS correctly. If you are using the SDK for your development then you need to run CCS Discovery of Porducts as described here:
processors.wiki.ti.com/.../Processor_SDK_RTOS_Setup_CCS
Also, refer to
Section 10.8 and 10.9 in the Training link porvided below:
Regards,
Rahul
Windows 10, CCS5.2, installed :xdctools_3_23_03_53, xdctools_3_23_04_60, xdctools_3_31_02_38_core, xdctools_3_32_00_06_core, xdctools_3_32_01_22_core;