Hello, I am having trouble connecting to the TI ARM+DSP processor on the EVMK2H board. I am using a XDS560v2 STM USB emulator. I am able to use the SD560v2Cnfg utility and it successfully is able to find a Emulator. I am trying to run the "platform_test_evmk2h" project. I have setup the Target Configuration and ran the Test Connection Toot. Here is its output:
[Start: Spectrum Digital XDS560V2 STM USB Emulator_0] Execute the command: %ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ C:\Users\JOE~1.LIN\AppData\Local\TEXASI~1\ CCS\ti\0\1\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 560/2xx-class product. This utility will load the program 'sd560v2u.out'. Loaded FPGA Image: C:\ti\ccsv6\ccs_base\common\uscif\dtc_top.jbc The library build date was 'Jul 27 2016'. The library build time was '17:21:41'. The library package version is '6.0.407.3'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. The controller has a version number of '6' (0x00000006). The controller has an insertion length of '0' (0x00000000). The cable+pod has a version number of '8' (0x00000008). The cable+pod has a capability number of '7423' (0x00001cff). This utility will attempt to reset the controller. This utility has successfully reset the controller. -----[Print the reset-command hardware log-file]----------------------------- The scan-path will be reset by toggling the JTAG TRST signal. The controller is the Nano-TBC VHDL. The link is a 560-class second-generation-560 cable. The software is configured for Nano-TBC VHDL features. The controller will be software reset via its registers. The controller has a logic ONE on its EMU[0] input pin. The controller has a logic ONE on its EMU[1] input pin. The controller will use falling-edge timing on output pins. The controller cannot control the timing on input pins. The scan-path link-delay has been set to exactly '2' (0x0002). The utility logic has not previously detected a power-loss. The utility logic is not currently detecting a power-loss. Loaded FPGA Image: C:\ti\ccsv6\ccs_base\common\uscif\dtc_top.jbc -----[The log-file for the JTAG TCLK output generated from the PLL]---------- Test Size Coord MHz Flag Result Description ~~~~ ~~~~ ~~~~~~~ ~~~~~~~~ ~~~~ ~~~~~~~~~~~ ~~~~~~~~~~~~~~~~~~~ 1 none - 01 00 500.0kHz - similar isit internal clock 2 none - 01 09 570.3kHz - similar isit internal clock 3 64 - 01 00 500.0kHz O good value measure path length 4 16 - 01 00 500.0kHz O good value auto step initial 5 16 - 01 0D 601.6kHz O good value auto step delta 6 16 - 01 1C 718.8kHz O good value auto step delta 7 16 - 01 2E 859.4kHz O good value auto step delta 8 16 + 00 02 1.031MHz O good value auto step delta 9 16 + 00 0F 1.234MHz O good value auto step delta 10 16 + 00 1F 1.484MHz O good value auto step delta 11 16 + 00 32 1.781MHz O good value auto step delta 12 16 + 01 04 2.125MHz O good value auto step delta 13 16 + 01 11 2.531MHz O good value auto step delta 14 16 + 01 21 3.031MHz O good value auto step delta 15 16 + 01 34 3.625MHz O good value auto step delta 16 16 + 02 05 4.313MHz O good value auto step delta 17 16 + 02 13 5.188MHz O good value auto step delta 18 16 + 02 23 6.188MHz O good value auto step delta 19 16 + 02 37 7.438MHz O good value auto step delta 20 16 + 03 07 8.875MHz O good value auto step delta 21 16 + 03 15 10.63MHz O good value auto step delta 22 16 + 03 1E 11.75MHz {O} good value auto step delta 23 64 + 02 3E 7.875MHz O good value auto power initial 24 64 + 03 0E 9.750MHz O good value auto power delta 25 64 + 03 16 10.75MHz O good value auto power delta 26 64 + 03 1A 11.25MHz O good value auto power delta 27 64 + 03 1C 11.50MHz O good value auto power delta 28 64 + 03 1D 11.63MHz O good value auto power delta 29 64 + 03 1D 11.63MHz O good value auto power delta 30 64 + 03 13 10.38MHz {O} good value auto margin initial The first internal/external clock test resuts are: The expect frequency was 500000Hz. The actual frequency was 499110Hz. The delta frequency was 890Hz. The second internal/external clock test resuts are: The expect frequency was 570312Hz. The actual frequency was 569214Hz. The delta frequency was 1098Hz. In the scan-path tests: The test length was 2048 bits. The JTAG IR length was 6 bits. The JTAG DR length was 1 bits. The IR/DR scan-path tests used 30 frequencies. The IR/DR scan-path tests used 500.0kHz as the initial frequency. The IR/DR scan-path tests used 11.75MHz as the highest frequency. The IR/DR scan-path tests used 10.38MHz as the final frequency. -----[Measure the source and frequency of the final JTAG TCLKR input]-------- The frequency of the JTAG TCLKR input is measured as 10.37MHz. The frequency of the JTAG TCLKR input and TCLKO output signals are similar. The target system likely uses the TCLKO output from the emulator PLL. -----[Perform the standard path-length test on the JTAG IR and DR]----------- This path-length test uses blocks of 64 32-bit words. The test for the JTAG IR instruction path-length succeeded. The JTAG IR instruction path-length is 6 bits. The test for the JTAG DR bypass path-length succeeded. The JTAG DR bypass path-length is 1 bits. -----[Perform the Integrity scan-test on the JTAG IR]------------------------ This test will use blocks of 64 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 0 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 0 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 0 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 0 All of the values were scanned correctly. The JTAG IR Integrity scan-test has succeeded. -----[Perform the Integrity scan-test on the JTAG DR]------------------------ This test will use blocks of 64 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 0 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 0 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 0 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 0 All of the values were scanned correctly. The JTAG DR Integrity scan-test has succeeded. [End: Spectrum Digital XDS560V2 STM USB Emulator_0]
I have the boot DIP Setting to 0010.
When I try to run the platform_test_evmk2h project I get the following reset error message:
If I change the boot DIP setting to 0001 I don't get this error message, BUT the program hangs at line 1114 platform_init().
Here is my project zipped up:
I have left the DIP setting to 0010 and tried removing the XCS200 but I get the same runtime error message about the processor in reset. The LCD on the board does say that it completing booting.
I am using the gel file "xtcievmk2x.gel" one DSP core 0.
Any ideas?
Thanks,
Joe