We have a custom board using the 66AK2E and are having trouble getting DDR3 to run properly at higher speeds. The board will sometimes hang when starting UBoot, usually at the point where it is transferring execution from Flash to DDR3. Other times the board will boot, but we are unable to transfer large files over Ethernet. Slowing the transfer rate down to 800MT helps this problem. However, we have experience problems at cold, likely due to the condition listed in the Errata. I have filled out the debug spreadsheet and tried to include it in this post. I am not sure that it was inserted properly. Any help would be appreciated.
Pat