Part Number: TCI6630K2L
Hi All,
I am using the BCP for for LTE Uplink. The test project given in the "pdk_keystone2_3_01_03_06" works fine for UL Test. Now I want to test it with my own input.
As a 1st step I am testing only SSL output.
I have created a test case with almost same parameters (Cell Id, RNTI, TB size, number of RB, modulation type etc). Tapped the output of the IDFT module on the reference C code what I have. And fed it to BCP. I have taken care of the partial de-interleave requirement of the SSL input here. I have verified it with hard coded indices in the input buffer instead of the actual IQ values for each symbol.
1. As a 1st step I have disabled descrambler also. Then when I check the SSL output I see that it has a sign reversal when compared my reference C code output for the same. i.e., when the reference output is +ve, SSL output is -ve and vice versa. Is there anything missing here..? Or is it expected..? Is there any setting to be changed to rectify this..?
2. Assuming this is expected (sign reversal), I enabled the descrambler for the same. Now the descrambled soft bits not at all matching in signs whether in normal mode or in sign reversal mode.
What am I missing here..?
I have used a SNR of 1 and a Q format of 0, and an RMS value of 1 hence my SSL output is +/- 127 for QPSK.
Please let me know if you need any other info.
Regards,
Ashok