Other Parts Discussed in Thread: LMK04828, CDCM6208, CDCM7005
Dear Champs,
My customer failed to work internal loopback test in their custom board although there was no issue in EVM.
They faced lack of PKTDMA buffer when they test it using PKTDMA , and it seemed it can not receive any packets over 2ms.
When they checked below resisters, it seemed this fail caused by UNSYNC frame. Could you please provide guide how they can debug this issue in their custom board?
They used aif2LteSingleToneK2HTestProject and aif2LteCheckRfK2HTestProject of pdk_keystone2_3_01_02_05.
gel file : C:\ti\ccsv6\ccs_base\emulation\boards\xtcievmk2x\gel\xtcievmk2x.gel
~~~~~~~~
Address: 0x1F50014 (RM_LK_STS0[0] Register)
EVM board (0x308)
FRAME_SYNC
custom board (0x1)
UNSYNC
Address: 0x1F50018 (RM_LK_STS1[0])
EVM board: (0x90000)
Number of Line Code Violations counted since last cleared and enabled: 0x9
Number of los_det, 8b10b code violation, occurrences in a master frame: 0x0
custom board: (0xFFFF000B)
Number of Line Code Violations counted since last cleared and enabled: 0xffff
Number of los_det, 8b10b code violation, occurrences in a master frame: 0xb
Address: 0x1F50020 (RM_LK_STS3[0])
EVM board (0x1000000)
Receiver FSM is in the HFSYNC state ST3
Custom board (0x2000000)
Indicates Loss Of Frame when the receiver FSM is in state ST0 or ST1.
Thanks and Best Regards,
SI.