Hello,
I see there are multiple options inside the Makefile located under C:\ti\pdk_c667x_2_0_4\packages\ti\boot\ibl\src\make.
If I want to build the IBL for NAND boot mode, should I explicitly say :
make evm_c6678_i2c ENDIAN=little I2C_BUS_ADDR=0x51 NAND=yes NAND_EMIF=yes ?
My second question is, what should the make command look like if i want to build the IBL for TFTP boot mode?
Thanks,
Viney