Hello,
I'm trying to test the uart example for I2C over NAND boot on c6678 evm and I see the following output on Teraterm :
IBL version: 1.0.0.17
IBL: DDR INITIALIZATION FAILED
IBL Result code 0K
Is there any configuration setting I'm missing? I tried both 666.7 and 333.3 MHz clock values for DDR3 but I get the same error in both cases.
Appreciate your help.
Thanks,
Viney