Other Parts Discussed in Thread: 66AK2L06, ADC12J4000, , DAC38J84
Hi,
I am using an ADC12J4000 EVM connected to the 66AK2L06 EVM via JESD204B interface directly.
There are no additional things connected to 66AK2L06 EVM.
The RFSDK version I'm using is 2.0.6 and the MCSDK version is 3.01.04.07.
To test the RFSDK, I followed the steps described in the RFSDK Installation Guide and selected the Wideband ADC12J4000 and DAC38J84 Demo as a Target board configuration.
I see errors when the RFSDK service launches. I paste the logs underneath:
Traceback (most recent call last):
File "/usr/bin/radio", line 108, in
command.onecmd(' '.join(sys.argv[1:]))
File "/usr/lib/python2.7/cmd.py", line 221, in onecmd
return func(arg)
File "/usr/lib/python2.7/rfsdk/command.py", line 1023, in do_reset
self.radio.radio_reset()
File "/usr/lib/python2.7/rfsdk/radio.py", line 1077, in radio_reset
self.dfe.dfe_reset()
File "/usr/lib/python2.7/rfsdk/platform/TCI6630K2L.py", line 454, in dfe_reset
res = self.rfsdkS.HwExceptionInit(req)
File "/usr/lib/python2.7/rfsdk/service.py", line 289, in HwExceptionInit
raise rfsdk.Error('rfsdkService.HwExceptionInit() API call failed with status %r (%d)' % (status, result,))
rfsdk.Error: rfsdkService.HwExceptionInit() API call failed with status 'RFSDK_API_RESULT_ERROR' (1)
In the target board configuration file - lamarr-evm-demo1-mcsdk3147, there are three UIOs - /dev/uio34, /dev/uio33, and /dev/uio32.
But on my board, the last UIO is /dev/uio32.
Please tell me what can I do to fix the error?
Best regards,
Gunzung Kim