Part Number: EVMK2H
Hello,
Is it possible to make L3 classify engine check only part of IP address? That is, to do '&' operation with subnet mask, then to check whether source & destination address for routing?
Thanks,
BK
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EVMK2H
Hello,
Is it possible to make L3 classify engine check only part of IP address? That is, to do '&' operation with subnet mask, then to check whether source & destination address for routing?
Thanks,
BK
Hello Eric,
Thanks for immediate reply.
Can I use Custom LUT1 for this purpose? From PA LLD APIs, there are 'PA_setCustomLUT1()' and 'PA_addCustomLUT1()'.
if byteMask[pa_NUM_BYTES_CUSTOM_LUT1] is applied to source & destination address as subnet mask, match[pa_NUM_BYTES_CUSTOM_LUT1] seems to be compared with the masked value.
Please check this is available.
Thanks,
BK