Tool/software: TI-RTOS
As discussed on an earlier thread, I have the UART behaving as I wish when I use PSKD 3.3. But the basis of my project remains on PSDK 2.2. I've tried to make my code as simple as possible. I am using callback mode and I am not using DMA. This works in the PSDK 3.3/CCS 7 environment. But I don't get the callbacks when build the same code using PSDK 2.2 in the context of my main project.
I'm thinking I need to update the UART library. I've tried pointing the project at the RTSC package for pdk_k2g_1_0_5. This results in a lot of undefined UART symbols. The build and library structure of 105 seems quite different from 101.
One thought is to replace the the UART source files with the newer source files and rebuild the library. But I don't see how the library rebuilds. Can you explain that? How do I go about rebuilding the UART library?
Or do you have a better suggestion?