I have an application where I would like to use SFPs to enable the choice of either copper Ethernet 10/100/1000BASE-T or fibre Ethernet 1000BASE-SX. The majority of copper SFPs I have seen require an SGMII interface running at 1.25Gbps where there is a PHY within the SFP which adjust the data rate to match the network by padding the SGMII link. However for fibre SFPs running 1000BASE-SX I dont believe there is a PHY - just a bidirectional electron to photon conversion and therefore the MAC needs to support 1000BASE-X.
Does the AM5K2E02 support SGMII and 1000BASE-X (802.3z) on its Gigabit (or 10GbE) Ethernet Subsystem for use with 1Gbps SFPs (to SFF-8074I)?
Or perhaps these two variants of SFP can be supported by the SRIO SERDES?