Hi,
Can anyone help me to find the address of SGMII registers in 66AK2L06 processor?
I understood that SGMII module is a part of GbE subsystem, and GbE is one of main components of NETCP. From memory map section of 66AK2L06 data manual, base address of NETCP configuration registers are 0x26000000.
GbE switch subsystem user guide(sprugv9d) gives the address offsets of SGMII port 1:4 modules.Offset of port1 SGMII module is given as 100h, where SGMII_IDVER register resides. So is it that the Address of SGMII_IDVER is 0x26000100? I verified the value at this address (after initialization using GEL file) and found that it is 0, instead of 0x4EC20101.
Is the calculation of actual register address correct, as mentioned above?
Regards,
Sreejaya