Other Parts Discussed in Thread: SYSBIOS
Tool/software: Code Composer Studio
There are a couple posts on this issue with older versions of code composer, but I have not been able to resolve this issue yet.
I need to create a new platform with XDCTools Version 3.32.1.22_core, however the RTSC->New Platform fails with the error below. If I attempt to create a new platform with the XDCTools version set to 3.50.1.12_core, it works properly. How do I get the 3.32.1.22_core option to work?
UPDATE/NOTE:
1) I have tried on various installation with the same problem, CCS 6.1, 7.0.0.00043, 7.1. all have the same issue. It seems to be following the XDCTools 3.32.1.22 Version.
2) I cannot upgrade to the XDCTOOLS 3.50 because we can't change compilers on this program. TI's site seems to indicate 3.50 is only good vor CCS7.1 and up, but we are stuck at 7.0.0.043 right now.
I attached a .txt file with my installation information (Help->About Code Composer Studio, Configuration Tab).