Hello,
Is it necessary to mount two 0.1 μF capacitors for VREFSSTL when C6657 does not have DDR3 memory?
Hardware Design Guide for KeyStone I Devices (SPRABI2C)
Figure 4 DDR3 VREFSSTL Voltage Divider
Regards,
Kazu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Is it necessary to mount two 0.1 μF capacitors for VREFSSTL when C6657 does not have DDR3 memory?
Hardware Design Guide for KeyStone I Devices (SPRABI2C)
Figure 4 DDR3 VREFSSTL Voltage Divider
Regards,
Kazu
Hello Yordan,
Thank you for your quick reply. Yes, I'll mount two 1 kΩ registers to divide DVDD15 and generate VREF (0.75 V) supply. Then I'll connect the VREF supply to the VREFSSTL pin. My question is whether I should mount two capacitors as below. I'm sorry for asking at minor things.
Regards,
Kazu
Kazu,
The detailed requirements for meeting the JEDEC requirements of the VREFSSTL do not need to be met when not using DDR. However, the absolute limits listed in the Data Manual must be met. Therefore, the voltage divider and the some filtering may be needed.
Tom
Amir,
This is not characterized but it is known to be a very low input current since the bias is created using two 10K ohm resistors in series and the end result is a voltage that is required to be within 1% of the midpoint voltage.
Tom
Hi Tom,
Thanks for your prompt response.
Do you know if there is a complete summary regarding Max currents per voltage-rails for the C6678?
(there is a summary table for the 6657 - https://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/204277/724947#724947)
Regards,
Amir
Amir,
That table shows pre-silicon estimates that are worst-case to support the EVM development for the C6657 EVM. This is stated in the post. Similarly, if you refer to the documentation for the C6678 EVM, you will see similar pre-silicon estimates that are worst-case to support the EVM development. However, these numbers are conservative estimates of current consumption published prior to power consumption characterization. Please refer to the C6678 Power Consumption Model (Rev. D) at: http://www.ti.com/lit/zip/sprm545 The general link for this is on the C6678 web page on TI.COM. This tool then provides a link to the Power Consumption Summary for KeyStone C66x Devices Application Report (SPRABI5B) at: http://www.ti.com/lit/an/sprabi5b/sprabi5b.pdf Proper use of this tool will provide maximum load current estimates based on your application requirements.
Tom