Tool/software: Code Composer Studio
I am debugging the communication between DSP and FPGA. I want to use GPIO as an interrupt input, scheduling DSP to read data from the FPGA; use EMIF CS2 as a data transfer interface. The initialization file configured with EMIF and GPIO; use the CFG file to configure the rising edge of the GPIO0 pin as an interrupt trigger. But now the program does not go into the function corresponding to the GPIO interrupt.
Is there any problem with this configuration? In addition to configuring EMIF and GPIO registers,do I also need to configure other registers, such as PSC, PLL?
This is our first contaction with the board 6678. Hope that experts would educate us!