Part Number: EVMK2H
Hi,
I am trying to implement the workaround for "SoC Power Failure" on the EVM board I just received. However, the python script fails with error message:
Traceback (most recent call last):
File "bmc_tool.py", line 377, in <module>
port_list = list_serial_ports()
File "bmc_tool.py", line 256, in list_serial_ports
s = serial.Serial(i)
File "build\bdist.win-amd64\egg\serial\serialwin32.py", line 31, in __init__
File "build\bdist.win-amd64\egg\serial\serialutil.py", line 218, in __init__
File "build\bdist.win-amd64\egg\serial\serialutil.py", line 264, in port
ValueError: "port" must be None or a string, not <type 'int'>
I have dug into the script, and I can force it to proceed by replacing a call to port_list = list_serial_ports() on line 377 with
port_list = []
port_list.append('COM3')
port_list.append('COM4')
Now I can get the GUI to come up. But when I do a "Get Versions" nothing happens
And if I try to load one of the UCD files, then the following stdout happens
Finished parsing and adding commands
Sending command: gpio d xxxx_x0xx
Delaying 2000 ms...
Sending command: gpio d xxxx_xxx0
Delaying 2000 ms...
Sending command: i2c 1.4E D2 04 01 04 10 40
and then I get a dialog box with error "An error has occurred with the BMC. Please power cycle the device and try again."