The usable USB port on DATASHEET(SPRS932E) with 66AK2G01 is listed as USB# 1
"The USB0 port is NOT supported in the 66AK2G01 device."
However, if you set 66AK2G01 with "TI PinMux" tool , the USB # 0 pin number(BALL NUMBER) will be valid.
Which USB port can be used with 66AK2G01? (USB# 0 or USB # 1)
Please also tell us the pin number (BALL NUMBER) of usable USB port.