Other Parts Discussed in Thread: RFSDK,
Hello again,
I am planning on running our JESD interface at 120MHZ which is different than the 122.88MHZ or 153.6MHZ that is listed in the
Recommended SerDes Register Configuration Options 6.3. the note below the table says
"TI requires customers to use TI-generated and supported, default PHY configurations for all
operating modes (supplied as part of MCSDK). TI cannot directly support customer
generated configuration files. The code/registers used and accessed in these configurations
must be considered as the "default" for a given interface use-case and must not be modified
by a customer."
Will I be able to correctly modify the JESD to use our 120MHZ reference and still use the MCSDK to do this? What code/registers will need to be changed from the "default" use case to accommodate the 120MHZ sampling rate?
thanks -b