Other Parts Discussed in Thread: CDCM6208V1, CDCM6208
Hi,
We are designing a 66AK2E05 custom board and we are using PLL settings different from the EVM board.
The EVM board has following clock frequencies:
NETCPCLK : 100MHz
DDRCLK:100MHz
CORECLK:100MHz
SGMII0CLK:156.25MHz
Whereas in our custom board, we have NETCPCLK: 125MHz and DDRCLK:125MHz; the CORECLK and SGMII0CLK are the same.
I have tested the initial bring-up on EVM board but wanted to make sure if bring-up will be fine even in our custom board. So, I wanted to change EVM's frequency to our custom board frequencies and test the initial boot-up. We are using UART bootmode initially and then use SPI bootmode.
Can you please tell me how can I change EVM's clock frequency to NETCLK:125MHz and DDRCLK:125MHz? Can it be done through U-boot or BMC?
Can you please advise the method to do this.
Regards,
Ashwini