Customer did test on over 20 TMS320C6678 boards and found that 2 out of the 20 boards consumed more 10 w than the others. After investigation, they found major power consumption was by core. CVDD power current of normal board is 8.5A but abnormal CVDD power current is 14.3A, as 6.3w more than normal board. Abnormal board CVDD1 consums 1.2w than normal ones. Could you please check and tell why this happened?
Since there are many bulk capacitor in switching power supply system, it takes time to shut down power. This is a relatively slow process. And DSP CVDD power and CVDD1 power can experience a temporary restart. Dose this phenomenon casue the current increase in the core ? Reference the attachment please.
The yellow lone is CVDD and the blue one is 5v to the board.