Tool/software: TI-RTOS
Hello all:
I remove the tftp module from the demo in the mcsdk_video_2_2_0_46\examples\transcode , add the SRIO drive module and rtp module into the project. The interlaced video (PAL 720*576 25fps) comes from a camera, and then is sent into DDR3 through SRIO. After the interlaced video is encoded by DSP, the generated stream is packeted with RTP protocol and sent out to PC. I choose mplayer to play the video. When I choose the following params
inputContentType = IVIDEO_INTERLACED
interlaceCodingType = 4
inputBufDesc->topFieldFirstFlag = 0
captureWidth =720
inputwidth =720
inputheight =288,
the pictures showed in the mplayer are 720*288, not the expected 720*576.
when I choose inputContentType = IVIDEO_PROGRESSIVE, no difference can be seen on the mplayer.
The question is what I need to do to make the interlaced video be encoded by the h.264 encoder.
Any suggestion will be appreiated!
Thanks!