The evaluation board has the following issues:
1) Upon powering up, most of the times indicates power failure. Sometimes it succeeds and boots.
2) To get access to any information demos etc, I need an IP address for the device on the same network that my computer is in. I followed the instructions that came with the box ( without connecting the computer through the USB bus) and the module displayed one, after a couple of tries, in my home private network. When the IP address was typed on the Browser of my PC, I was getting errors, like too much time to connect.
I tried again, this time following the video on the link https://training.ti.com/introducing-the-evmk2h-evaluation-module that shows that the module has to be connected to the computer through the USB. The module does not display the IP address anymore. On my modem's network map the connection was shown broken. To fix the problem, I removed the device from that map and tried to boot again hoping that the modem may issue another one for the board but it did not. According to the start up guide, I cannot do anything unless I successfully complete the above step. Can anybody help?
Evi.