Hello,
We are facing an issue that, for the first power up, uBoot stops at DDR3 0-bytes.
Prints are -
U-Boot 2017.01 (Oct 05 2017 - 19:52:37 +0530)
CPU: 66AK2Ex SR1.0
Model: Texas Instruments Keystone 2 Edison EVM
I2C: ready
DRAM:
Clear entire DDR3 memory to enable ECC
0 Bytes
After power cycle the board, the board boot properly with prints -
CPU: 66AK2Ex SR1.0
Model: Texas Instruments Keystone 2 Edison EVM
I2C: ready
DRAM:
Clear entire DDR3 memory to enable ECC
2 GiB
NAND: 512 MiB
Net: Could not get PHY for ethernet-mdio: addr 0
Warning: netcp@24000000 using MAC address from ROM
eth0: netcp@24000000Could not get PHY for ethernet-mdio: addr 1
Warning: netcp@slave-1 (eth1) using random MAC address - 66:b9:4b:02:27:25
, eth1: netcp@slave-1
Warning: netcp@slave-2 (eth2) using random MAC address - a6:8e:bf:19:e4:c1
, eth2: netcp@slave-2
Warning: netcp@slave-3 (eth3) using random MAC address - 82:3d:58:d6:ed:49
, eth3: netcp@slave-3
Warning: netcp@slave-4 (eth4) using random MAC address - 86:46:f4:04:c8:69
, eth4: netcp@slave-4
Warning: netcp@slave-5 (eth5) using random MAC address - 26:31:75:40:81:13
, eth5: netcp@slave-5
Warning: netcp@slave-6 (eth6) using random MAC address - 5a:fc:97:02:06:f2
, eth6: netcp@slave-6
Warning: netcp@slave-7 (eth7) using random MAC address - d6:1f:8b:42:ef:73
, eth7: netcp@slave-7
Hit any key to stop autoboot: 3
sometimes we need to power cycle the board multiple times, sometime for the first time itself board boot properly.
can any tell me that what are the possible reasons behind this behavior.
Thanks and Regards
Tarang Jindal