Hi to all,
we were using MT41K256M16HA-125:E (DDR3-1600) on a previous release of a custom DSP TMS320C6678 based board.
The memories were working at 1066Mbit (533Mhz) without issues.
Those memories are now obsolete, so we need to replace them with the following suggested part number: MT41K256M16TW-107 IT:P (DDR3-1866).
Are those new devices supported using the same working frequency (1066Mbit i.e. 533Mhz) as the previous used ones?
On sprabi1b.pdf (DDR3 design requirements for keystone devices) there are no mention relating to DDR3-1866 devices.
Thanks in advance,
Simone