Other Parts Discussed in Thread: RFSDK, ADC12J4000
We have a wideband receiver application that we are currently running on a C6678 with an expensive FPGA doing DDC and tuning at 200 MSPS (I/Q). We are considering using the 66AK2L06 with ADC12J4000 with a single antenna instead. I can work with the supported rates of the RFSDK. I am unclear of what the limitations of data throughput are when using the DFE in a single antenna receiver application.
Using the supported rate of 368.64 in bypass mode, does this mean I can get packet DMA of 368.64 MSPS (16 bit I/Q) data direct to one of the C66x cores? If using a single DDUC, what is the max rate?
Thanks,
Dan