Part Number: EVMK2G
Tool/software: Code Composer Studio
Hello Everyone!
I'm in the process of learning how to work with TI-RTOS on the K2G Evaluation board.
I created a new project in CCS 7, using SYS/BIOS 'typical' template (on the C66 core).
At first, I added a new task and tried to output from it some words to the console - that worked fine.
After that, I tried to add some GPIO capabilities by including the 'ti/drv/gpio/GPIO.h' file. But here is the thing - when I try to use one of the functions included in that file I get errors by the compiler.
Same happened to me when I tried to include "ti/board/board.h" file and use 'Board_getIDInfo(...)' function.
The errors are:
#10010 errors encountered during linking; "RTOS_Test_3_C66.out" not built
#10234-D unresolved symbols remain
gmake: *** [all] Error 2
gmake[1]: *** [RTOS_Test_3_C66.out] Error 1
It seems like a linker error but I'm not sure. I checked the project's properties and looked over the including paths and everything is in place.
I must note that i'm new to RTOS' concepts and also to TI's driver APIs.
I would like to get some help solving that issue.
Thanks,
Dor