I've got an image that was built to boot from SPI Flash. This image boots from SPI with no issues when burned to the SPI Flash of the Eval board, with the jumpers set to boot from SPI. However, on our custom board, the image does not boot up. I've connected to the target with code composer and I can see that the processor is stuck in a big loop in the RBL between addresses 0x20b0a26c and 0x20b0a338. Can someone tell me what the RBL is not happy about? I've read the DEVSTAT register and it seems to be correct. I can also run code (from CCS) on the target that reads and writes to SPI flash with no problems. Oh, and I can also run the same image from CCS on the target that I'm trying to boot from SPI and it runs okay.