Tool/software: Code Composer Studio
Hi TI engineer:
We have a C6655 board, which have a pcie port to be put in pcie slot of the PC Motherboard. We put the board in the slot and make sure that connection is good. The we load a program to init the pcie port.But the program stuck at here:
We check the register status of debug0:
It shows that the ltssm_state is not in L0.So link trainning isn't made through.
We try a full reset, but it doesn't make any difference.The connection can't be built.
Software environment: CCS 5.5+bios_mcsdk_02_01_02_06
The program used to init the pcie have been attached. So does the gel we use to init the pll and ddr
Could you help us on how to solve this problem? How to make c6655 connect to PC? Thank you very much.DSP_C665x.gelCould you give us some g