Part Number: TCI6630K2L
Hello,
So I have been able to get the RFSDK up and running with LTE packets moving my data in and out throught the DFE. My next challenge now is getting our own custom packet sizing to work instead of LTE packets. I have noticed there are 4k configurations included with the RFSDK but I previously had my design working with the LTE60 Demo1 configuration which uses the lower speed JESD lan (4.9 GHz) it appears like the 4k configurations for the dfe only say they support the higher speed lane rate. Would I be able to use the same tgtcfg file from the LTE60 configuration with the 4k Demo1 config in order to get the lower lane rate as that rate is required by our design? Does the DFE tgtcfg file have anything to do with what size of data packets are being transmitted?
Thanks so much,
Ken Witham