Tool/software: TI-RTOS
Hi,
I have an application (running on both arm and dsp core) which works perfectly when I run it using JTAG debugger. But when I flash the same to QSPI Flash, it does not work at all.
I have followed the following link to flash my binary on the board: http://processors.wiki.ti.com/index.php/Processor_SDK_RTOS_BOOT_K2G
According to the link I should generate the app and flash it through QSPI. Interestingly when my app is of smaller size, it works as intended. But if I add some modules to my application, thereby increasing the size of app, it stops working.
Note that QSPI flashing works properly irrespective of the size. Its just that after booting in QSPI mode, the application does not work properly when app size is little bigger.
My application is built using Processor SDK.
Thank You