Hi,
I am getting this error while loading my .out into 66AK2G02.
C66xx: Trouble Reading Memory Block at 0x76d7bb76 on Page 0 of Length 0x1: (Error -1202 @ 0x76D7BB74) Device core is hung. The debugger will attempt to force the device to a ready state to recover debug control. Your application's state will be corrupt. You should have limited access to memory and registers, but you may need to reset the device to debug further. (Emulation package 6.0.576.0)
I am using CCSv7. I am using external JTAG spectrum digital XDS560v2 STM USB Debugger. Target is getting connected successfully.
GEL files are executed successfully as shown below:
C66xx: GEL Output: PLL has been configured (24.0 MHz * 100 / 1 / 4 = 600.0 MHz)
C66xx: GEL Output: ARM PLL has been configured with ref clock 24MHz, -sysclkp_period 41.6666 (24.0 MHz * 100 / 1 / 4 = 600.0 MHz)
C66xx: GEL Output: Power on all PSC modules and DSP domains...
C66xx: GEL Output: Power on PCIE PSC modules and DSP domains... Done.
C66xx: GEL Output: UART PLL has been configured (24.0 MHz * 128 / 1 / 8 = 384.0 MHz)
C66xx: GEL Output: NSS PLL has been configured (24.0 MHz * 250 / 3 / 2 = 1000.0 MHz)
C66xx: GEL Output: ICSS PLL has been configured (24.0 MHz * 250 / 3 / 10 = 200.0 MHz)
C66xx: GEL Output: DSS PLL has been configured (24.0 MHz * 198 / 12 / 16 = 24.75 MHz)
C66xx: GEL Output: DDR PLL has been configured (24.0 MHz * 133 / 1 / 16 = 199.5 MHz)
C66xx: GEL Output: XMC setup complete.
C66xx: GEL Output: DDR3 PLL Setup ...
C66xx: GEL Output: DDR3 PLL Setup complete, DDR3A clock now running at 400MHz.
C66xx: GEL Output: DDR3A initialization complete
But after loading the .out file I am getting the error.
I am not able to understand what's going wrong.
Can somebody help?
With regards