Is there a BOM available somewhere for the 6678 EVM? In particular what's the part number for the DDR3?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a BOM available somewhere for the 6678 EVM? In particular what's the part number for the DDR3?
The BOM is not yet available for the C6678 EVM. The C6678 EVM is designed to support a full 72-bit memory topology (includes ECC bits) using JEDEC-compliant DRAM devices. It is implemented using x16 DRAM devices for the data and either a x16 or a x8 DRAM device for the ECC memory. Initial EVMs will be populated with 1Gb or 2Gb DRAMs from Samsung, Micron or Elpida. Possible part numbers are SAMSUNG K4B2G1646C-HCH9 or Elpida EDJ1116BBSE-DJ-F.