• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » C6000 Multicore DSP » Keystone Multicore Forum (C66, 66A, AM5) » All Tags » Ethernet
Share
C6000 Multicore DSP
  • Forums
  • Announcements

Browse by Tags

C6000 Multicore DSP

Welcome to the C6000 Multicore DSP Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
Ethernet
  • 6678
  • 6678EVM
  • 6678l
  • 6678le
  • boot
  • C6670
  • C6678
  • C6678EVM
  • C667x
  • C66x
  • C6778
  • EMAC
  • EVM6670l
  • EVM6678
  • EVM6678LE
  • EVMC6678
  • EVMC6678L
  • MCSDK
  • NDK
  • NETCP
  • PA
  • PCIe
  • SGMII
  • TMS320C6678
  • TMS320C66x
Related Posts
  • Forum Post: Re: TMS320C66x EMAC IEEE1588 support

    Derek Brown Derek Brown
    Igor, The GbE switch user guide has been updated to provide more information about the time synchronization module. It will be available for download in the near future. The document with the updates will be marked as revision A. Regards, Derek
    on Jun 30, 2011
  • Forum Post: Secondary Boot with PLL fix

    Jim Rondero Jim Rondero
    Hello, In order to perform Ethernet boot, I wish to program the i2c eeprom on my EVM with the secondary boot example instead of the IBL. When running the secondary boot in debug mode it works a sends the BOOTP package as expected. But when I use the make file supplied and program it to the eeprom...
    on Jul 5, 2011
  • Forum Post: Re: Intercepting Ethernet frames

    Derek Brown Derek Brown
    Chiang, If you want to use the EMAC CSL APIs, please see try the EMAC example installed with the PDK. This will show you how to setup the EMAC using the CSL with the C6670. On my PC, the project was installed in the following location: C:\Program Files\Texas Instruments\pdk_C6670_1_0_0_9_beta2...
    on Aug 24, 2011
  • Forum Post: UDP fragmented messages

    Jim Rondero Jim Rondero
    Hello, I'm using a c6678 evm and trying to send and receive fragmented messages (larger than1472), While trying to send buffer larger than 1472 I receive the following message in the console window: "E_spOutOfBounds stack error, SP = 0x800654e0. While trying to receive a fragmented...
    on Oct 5, 2011
  • Forum Post: Re: C6678, Configuring Ethernet

    Derek Brown Derek Brown
    Greg, It looks like you are referencing the correct documentation, so you might find some example code helpful. The SYSBIOS MCSDK contains a simple example for configuring the Ethernet. If you haven't already downloaded the MCSDK, you can download it from this website: http://software-dl.ti...
    on Oct 12, 2011
  • Forum Post: C6670 external loopback not working for packet size < 60 bytes

    Robert Buranyi Robert Buranyi
    Hello, I am testing the 6670EL EVM and checking the sources from the latest MCSDK. (MCSDK 2.0.3.15 + CCS 5.0.3, Win32). I am using the PA_emacExample from there. My EVM is connected the a Gbe switch that is connected to a PC. I am checking first the transmission path from EVM to PC, and I face a problem...
    on Nov 3, 2011
  • Forum Post: [TCI6618/6616] Boot parameter table of two-level bootloader using I2c and Ethernet

    Eric Liang Eric Liang
    Hi all, I am working on TCI6618's bootloader using I2c and Ethernet. But I can NOT make out the correct boot parameter table of Ethernet boot. By reading the user guide of bootloader (2011 version), there are several parameters not found in the GbE user guide, such as SGMII Rx / Tx / Aux Cfg register...
    on Nov 4, 2011
  • Forum Post: MCSDK C6670 PDK NIMU Eth transport driver bug

    Simon Locke Simon Locke
    Hi, As part of my work getting an Ethernet bootloader going (in conjunction with: http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/126829/541935.aspx#541935 ) I'm trying to get a stack shutdown going with a call to NC_NetStop. I believe I've found a bug in the C6670 PDK 1.0.0...
    on Nov 30, 2011
  • Forum Post: Re: C6678 – emac loopback example on the EVM board - PA question

    Derek Brown Derek Brown
    Yatsir, Are you trying to power down NetCP between runs to emulate some sort of power down state, or are you simply looking for a way to execute the example multiple times without having to power down the EVM? If it is the latter, then after executing the example code, then you should be able to do...
    on Jan 25, 2012
  • Forum Post: Re: C6678 – emac loopback example on the EVM board - PA question

    Derek Brown Derek Brown
    Yatsir, With respect to this comment: “ I want that my application will power down and then power up the NetCP every run (to simulate rerunning the application on the C6678 without power down the entire CPU).” After digging a deeper into the procedure for powering down the PASS power...
    on Jan 31, 2012
  • Forum Post: Re: Unable to reach Gigabit Ethernet Switch Subsystem registers

    Derek Brown Derek Brown
    Koray, It sounds like the power domain for the NetCP may not be getting turned on successfully. I have attached a GEL file that you can use to get the status of the Power Sleep Controller Registers. (Please visit the site to view this file) After you run your application and notice a failure...
    on Jan 31, 2012
  • Forum Post: Re: Unable to reach Gigabit Ethernet Switch Subsystem registers

    Derek Brown Derek Brown
    Koray, I am glad to hear that your setup is working now. Was 312.5 MHz clock that you were showing in the scope captures the input for the SGMII SerDes PLL? Did you make any other changes to your setup? Although the SGMII SerDes input clock could prevent the SGMII and SerDes interfaces from...
    on Feb 1, 2012
  • Forum Post: Re: Giga ETH Application within C6678

    Derek Brown Derek Brown
    Gideon, I am not familiar with the software examples that you are referring to, so I cannot tell you which project would be best for starting your project; however, I can answer some of your questions. 6 ) At TCP/IP I guess the packet length is 8192 Bytes .Is it min ? or max ? I am not sure...
    on Feb 10, 2012
  • Forum Post: Re: Problem with MDIO link status register on C6678 EVM board

    Derek Brown Derek Brown
    Jochen, Can you please measure the frequency at the SYSCLKOUT pin (pin AE3). You can use test point 12 (TP12) on the EVM to measure this signal. This is the same DSP/6 clock that is used for MDIO input clock, and should be 166.67 MHz for 1 GHz CPU operation. Before measuring this pin, please make...
    on Feb 27, 2012
  • Forum Post: Re: Ethernet not working after link has been down

    Derek Brown Derek Brown
    Gertjan, It is unlikely that what you have described is the QMSS stall error. However, to avoid this issue, you should use internal linking RAM (recommended unless you need more than 16K descriptors) or put the descriptors and linking RAM in different locations. After the link comes back up, are...
    on Feb 28, 2012
  • Forum Post: Re: Ethernet not working after link has been down

    Derek Brown Derek Brown
    Gertjan, Since you are seeing the statistics update, then that means that the packets are getting into the Ethernet switch. Are the packets getting out of the Ethernet Switch? If you are not sure, then use can use the following procedure: After you encounter the issue, please halt your program...
    on Mar 1, 2012
  • Forum Post: Re: Ethernet not working after link has been down

    Derek Brown Derek Brown
    Gertjan, I am glad to hear that you were able to resolve this issue. From a hardware perspective, this bit does not need to be set if software is going to be setting up the speed and duplexity of the EMAC and SGMII modules. This bit only needs to be set if the EMAC needs to get the speed and duplexity...
    on Mar 12, 2012
  • Forum Post: Re: Problem with MDIO link status register on C6678 EVM board

    Derek Brown Derek Brown
    Jochen, Is your code enabling the EXT_EN bit in the MAC Control register? I found this post where someone was having trouble with the link when the EXT_EN bit was set, and the issue went away when the EXT_EN bit was cleared.
    on Mar 13, 2012
  • Forum Post: Re: evm C6678 board network seems work on only half duplex mode

    Derek Brown Derek Brown
    Lucifar, The C6678 hardware has been tested and verified to handle 1000 Mbps of TX unicast traffic (2000 Mbps multicast traffic) and 2000 Mbps of RX traffic simultaneously. Please see section 8 of the Keystone Throughput Performance Guide ( SPRABK5 ). There could be many different things to explain...
    on Mar 13, 2012
  • Forum Post: 6678EVM ethernet reception

    Pratheek Suresh Pratheek Suresh
    i want to try UDP packet reception and transmission in sysbios environment, is there sample codes vailable in the NDK ? please provide me with the link to go further
    on Mar 15, 2012
  • Forum Post: Re: C6678 - MCSDK - drivers support for Jumbo frames

    BhavinKharadi BhavinKharadi
    Hi, PA LLD inside MCSDK supports Jumbo frames. You also have to configure P0_RX_MAXLEN, EMAC1 RX_MAXLEN and EMAC2 RX_MAXLEN registers in your application from switch sub-system to allow the jumbo frames to be received and sent out from switch sub-system. Regards, Bhavin
    on Mar 19, 2012
  • Forum Post: Ethernet boot loading 6678

    Greg Reuter Greg Reuter
    Hi, Can I boot DSP6678 from Ethernet (BootP) without booting from something else (I2C) first? On or board, currently in schematic capture, we’re going to connect SGMII directly to another microprocessor’s SGMII (no PHY), and plan to boot from Ethernet. My TMDXEVM6678L (1.0) won’t...
    on Mar 15, 2012
  • Forum Post: Re: EVM6678L: POST ethernet test - packet not transmitted on the cable

    BhavinKharadi BhavinKharadi
    Hi, It looks like you are trying to get the bare minimum code to get the packet transfer on ethernet so that you can add that to your POST, is my understanding correct? Before doing SGMII, are you configuring the SERDES? Also before configuring SERDES, are you enabling ethernet switch sub-system...
    on Mar 22, 2012
  • Forum Post: Re: Using C6678 simulator with NDK Library to access Socket

    BhavinKharadi BhavinKharadi
    Saurabh, Simulator is using WinPcap to do the communication. Now as you are able to ping to the simulator, what do you want to use WinPcap for? Regards, Bhavin
    on Mar 22, 2012
  • Forum Post: Using C6678 simulator with NDK Library to access Socket

    Saurabh Kumar Singh Saurabh Kumar Singh
    Hello everyone!! I have been stuck with a small task that i have been trying to do, for almost 10 days now. Since i am running out of time and options, i thought of posting it here. With so many knowledgeable members in one place, im sure i'll get guidance in the right direction. To explain...
    on Mar 13, 2012
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use