Application : Video Server
DSP : TMS320DM368ZCE
OS : Linux 2.6.1.8
Questions : I've already tried applying the Register & patch thru web_link download file.
It's working to Embedded sync with BT656 by the applied patch about ISP file(linux driver) & 5158 video.
Pls let me know how to set the register?
(needed in order to do loading the 4CH video)
main issues :
sometimes, occurred system hanging at video decoder line(tvp5158) in field,
be twisted 4byte discript at that time,this issue are reappeared 1time of 100 times test after the video signal plug on/off repeat..after failed, and then If reboot, It's recovered and normal worked.
1) disconnected TVP5158 device :
- If repeat the connected camera signal by attach and detach, TVP5158 is disconnected.
- It’s very difficult to find the location of Log(about bugs).
- If needed, I will send the register data in normal status and adnormal status.
2) output video is bent :
- bent video at the upper location( around 5%)
- How about Z-matching? ( 75ohm, now)
- If any check point, let me know?
3) TVP5158 latest patch was upto "c" version only,
- Why dose not updated to patch “D” or “E"? what is the reason?
- pls check below TVP5158 chip version?
- Is it available to update version?
“$NA 98A1GHW G4”
Request Items :
1) real working LSP Driver in EVM.
2) TVP5158 I2C Register Setting Source Code.
3) final Patch(2.2.58) with proven normal working in EVM.
regards,
KIM