Hi,
I have an image sensor (MT9M114) with VDDIO=2.8V that is connected directly to PCLK & C[7:0].
Is there any issue using VDD_ISIF=2.8V?
The DM365 datasheet only talks about 1.8V or 3.3V.
If not, what's the closest voltage to 2.8V VDD_ISIF can work with?
Thanks,
YC
Sorry for bringing up this old thread, but I have the same problem. We would also like to use a sensor that has 2.8V I/O with the DM365.
I would like to tie the DM365 VDD_ISIF rail to 2.8V. Does the DM365 distinguish between 1.8V and 3.3V? Or is the power domain isolated and operate with 2.8V, given VIH / VIL are scaled accordingly?
JPM