Hi all,
I don't know whether it is the right forum to ask such a question.
Is DM368IPNC Appro reference design(both in hardware and software) can be adapted to make a
PTZ camera.Currently this software works fine for box type camera.
what changes need to be done in hardware and software in order to convert it into
a PTZ camera.
Practically the major difference b/w dome and PTZ camera is that in PTZ camera there is a facility of
manual tilt and zoom in/out.If anyone can tell that the Appro IPNC software takes care of this feature
or we have to add/integrate this feature to the existing software.
Thanks and Regards,
Mayank
There is RS485 interface available on the camera, you might think of implementing pelco-D protocol on ARM and have this feature
Regards,
Raghu
Please mark this reply as Verify Answer on this post if it answers the question.
Hi,
I want to use PTZ in my design.Kindly guide me to implement same in DM368IPNC Appro reference design.Which function or files need to modify to enable/access ptz facility.
Regards
Samir Mistry