This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[DM388] Power dashboard issue about DDR3.

Hi Ti:

We have seen dm385 power dashboard below.

http://processors.wiki.ti.com/index.php/File:DM385_PowerSpreadSheet_Ver1_00_Release.zip.

Just a question for it.

Does this power dashboard has include DDR power consumption or DDR controller only?

In deep sleep mode, EMIF_0 is 15mW only.

DVDD_DDR becomes 0mW in deep sleep mode.

But DDR need to stay in self refresh mode.

We don't understand why DVDD_DDR can  become 0mA in deep sleep mode.

Thanks

DarkHou

  • Hi Dark,

    dark hou

    DVDD_DDR becomes 0mW in deep sleep mode.

    But DDR need to stay in self refresh mode.

    We don't understand why DVDD_DDR can  become 0mA in deep sleep mode.

    The DM38x device really do not have any power consumption from DVDD_DDR power rail in deep sleep mode. EMIF_0 15mW are coming from CVDD power rail.

    But keep in mind that DDR memory chips have their own power consumption in self-refresh mode. This consumption will be added to DVDD_DDR and you have to check for this consumption in DDR memory chip datasheet.

    Regards,
    Pavel



This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.