Linux/TMDSCSK388: Problems with creating SD card for DM388 camera kit

Part Number: TMDSCSK388

Tool/software: Linux

Hello,

I have modified some configuration options and have compiled using 'make syscal all'. I am trying to write to the SD card as per the steps explained in http://processors.wiki.ti.com/index.php/IPNC_RDK_DM38x_,_DM8127#Boot_setup_for_custom_build.

root@ubuntu:~/ti/ipnc_rdk-3.9.1/Utils/sd-script# ./mksd-ti81xx.sh /dev/sdb  ../../Source/ipnc_rdk/tftp/DM388/sd/MLO  ../../Source/ipnc_rdk/tftp/DM388/sd/u-boot.img ../../Source/ipnc_rdk/tftp/DM388/sd/dm38x-csk.dtb ../../Source/ipnc_rdk/tftp/DM388/sd/uImage ../../Source/ipnc_rdk/target/filesys.tar.gz 
All data on /dev/sdb now will be destroyed! Continue? [y/n]
y
[Partitioning /dev/sdb...]
unmounting device '/dev/sdb'
1024+0 records in
1024+0 records out
1048576 bytes (1.0 MB, 1.0 MiB) copied, 0.896747 s, 1.2 MB/s
DISK SIZE - 15987638272 bytes
CYLINDERS - 1943
sfdisk: invalid option -- 'D'
Try 'sfdisk --help' for more information.
[Making filesystems...]
[Copying files...]
mount: /mnt: special device /dev/sdb1 does not exist.
umount: /dev/sdb1: no mount point specified.
mount: /mnt: special device /dev/sdb2 does not exist.
umount: /dev/sdb2: no mount point specified.
[Done]

Here is the script file as provided in the IPNC rdk software. ( I have not modified this script)

#!/bin/bash

if [[ -z $1 || -z $2 || -z $3 || -z $4 || -z $5 || -z $6 ]]
then
        echo "mksd-ti81xx Usage:"
        echo "  mksd-ti81xx <device> <MLO> <u-boot.img> <dtb> <uImage> <rootfs tar.gz>"
        echo "  Example: mksd-ti81xx /dev/sdc MLO u-boot.img dm38x-csk.dtb uImage nfs.tar.gz"
        exit
fi

if ! [[ -e $2 ]]
then
        echo "Incorrect MLO location!"
        exit
fi

if ! [[ -e $3 ]]
then
        echo "Incorrect u-boot.img location!"
        exit
fi

if ! [[ -e $4 ]]
then
        echo "Incorrect dtb location!"
        exit
fi

if ! [[ -e $5 ]]
then
        echo "Incorrect uImage location!"
        exit
fi

if ! [[ -e $6 ]]
then
        echo "Incorrect rootfs location!"
        exit
fi

echo "All data on "$1" now will be destroyed! Continue? [y/n]"
read ans
if ! [ $ans == 'y' ]
then
        exit
fi

echo "[Partitioning $1...]"

DRIVE=$1

for i in `ls -1 $DRIVE?`; do
 echo "unmounting device '$i'"
 umount $i 2>/dev/null
done

dd if=/dev/zero of=$DRIVE bs=1024 count=1024

SIZE=`fdisk -l $DRIVE | grep Disk | awk '{print $5}'`

echo DISK SIZE - $SIZE bytes

CYLINDERS=`echo $SIZE/255/63/512 | bc`

echo CYLINDERS - $CYLINDERS
{
echo ,9,0x0C,*
echo 10,,,-
} | sfdisk -D -H 255 -S 63 -C $CYLINDERS $DRIVE

echo "[Making filesystems...]"

mkfs.vfat -F 32 -n boot "$1"1 &> /dev/null
mkfs.ext3 -L rootfs "$1"2 &> /dev/null

echo "[Copying files...]"

mount "$1"1 /mnt
cp $2 /mnt/MLO
cp $3 /mnt/u-boot.img
cp $4 /mnt/
cp $5 /mnt/uImage
umount "$1"1

mount "$1"2 /mnt
tar zxvf $6 -C /mnt &> /dev/null
chmod 755 /mnt
umount "$1"2

echo "[Done]"
                     

In the script in Line 9:

for i in `ls -1 $DRIVE?`; do

 Is the  '?' required. I tried removing the '?' and I still have the same issue.

For some reason sdb1 and sdb2 are not created. However 'lsblk' shows '/dev/sdb'

Does anyone have a hand on this issue?

11 Replies