• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors » DM3x DaVinci Video Processor Forum » New binning or skipping mode.
Share
DaVinci™ Video Processors
  • Forums
  • Announcements
Options
  • Subscribe via RSS

Forums

New binning or skipping mode.

This question is not answered
JamesS
Posted by JamesS
on Jul 25 2008 00:16 AM
Prodigy190 points

Hi,

 I would like to change the binning or skipping modes available.  At the moment I see in  drivers/media/video/mt9p031.c that in static int mt9p031_setBinning_Skip(int arg) {} there are bits set and cleared that affect the sensor row and column settings at the same time.

  I need to add options to skip or bin rows but not columns.  That is to leave the image width the same, but reduce the height by a factor of 2.

 Also I need to add variable frame rates, so the frame rate can be adjusted from about 80 FPS to 200 FPS.  The 200 FPS can only occur with binning or skipping, so the data throughput is not too high.

 What do I need to modify in the kernel?  Will this affect the DVSDK?  If so how, and will it cope?

 Is this even possible with the current mvl kernel and Ti dvsdk?

James. 

 

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Juan Gonzales
    Posted by Juan Gonzales
    on Jul 25 2008 09:36 AM
    Mastermind33965 points

    I am not too familiar with micron sensor driver (or hardware capabilities yet), so I cannot comment much on binning or skipping rows, but if you are going to be changing frame rates, you need to take pixel clock (aka video clock) into account.

    pixel clock = resolution x refresh rate

    By default, the video input clock to DaVinci is 27MHz (enough for NTSC D1 @ 30fps), if you do not change the resolution and change the refresh rate, then your pixel clock needs to change.  Many of our DaVinci parts (DM355, DM644x,...) can take input video clocks up to 75Mhz.  The question is, do you have the hardware in place to provide such a pixel clock.

    The beautiful thing about Linux is that is open source and you have all the software driver source code at your disposal; therefore, as long as the hardware capability is present, you can certainly achieve this via the kernel provided in the DVSDK. 

    VPFE DaVinci CCD
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Bernie Thompson TI
    Posted by Bernie Thompson TI
    on Jul 25 2008 09:41 AM
    Mastermind41680 points

    Looking in the LSP included with the last couple of DM355 DVSDK releases (1.30.00.40 and 1.30.00.23) I am not seeing the /drivers/media/video/mt9p031.c file, rather there looks to be a mt9t001.c file that does not have the binning function you mention, so I am curious what kernel source tree you are using?

    As long as the drivers are modified properly I do not see any reason to modify anything else in the kernel for something like this, as everything that would be changing would be at the driver level. Of course the application would also have to agree on the image size (the DVSDK demos may get confused by this), as well as be able to handle the frames at the rate you want, but the real work would be getting the settings right in the sensor and adjusting the buffers in the driver to handle the proper sizes.

    VPFE
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • JamesS
    Posted by JamesS
    on Jul 25 2008 16:58 PM
    Prodigy190 points

    We have an IP Net Cam from Appro.  It has this extra source file in it's kernel sources.

     I see some code in the application, that shoves a binning set function pointer into a structure, that seems to be passed to an Appro closed source AEW library.  The code path has been a little hard to follow.  But this is why I wonder what else is going on behind the scenes, and possibly in the DVSDK.

     In the kernel, some of the binning funtions are called from a dm355_vpfe.c (or similar - I don't have the code at home ;-).

    I guess part of my problem is that I don't know where the DVSDK components begin and end, and what they affect and how.  Can you guys recommend some good reading?

    I also wonder what else a change of resolution would affect, when the resolutions and frame rates are given as fixed enumerated constants, like VGA_30FPS.  If I wanted 640x496 for example, what else needs to know besides the sensor - via i2c?  I presume the iPipe, and probably the MPEG engine.  Ah - I've spent too long looing at code, my mind is a mess.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Juan Gonzales
    Posted by Juan Gonzales
    on Jul 25 2008 17:47 PM
    Mastermind33965 points

    DVSDK software is what is available from TI via our software update site; this software is primarily written and controlled by TI.  In addition, we have teamed up with many 3rd parties in order to provide more readily available solutions to our customers.  Appro is an example of one such third party.

    Unfortunately, 3rd parties often branch off one of our DVSDK software releases and end up providing their own software implementation which closely resembles and often overlaps our DVSDK software.  I am not familiar with Appro's software deliverables, but it sounds like they have branched off one of our DVSDK Linux kernels and changed portions of the Linux kernel and deliver their own kernel version to customers.  Latest DVSDK has drivers (including source code) for AEW (as opposed to libraries provided by Appro) and supports a couple of Micron sensor daughter cards (off-the-shelf).  TI has more control over this more generic solution as a starting point for customers that need to interface to CCD sensors.  The Appro offering is a more complete IP Net Cam solution, but it also depends on software written and supported by Appro which TI does not always have insight into.  Therefore is hard to judge how much of the original DVSDK is kept by Appro solution and how much is replaced by their own implementation (or even what DVSDK version they based their solution on and do they plan on upgrading to newer DVSDKs as they become available).

    As far as making changes to resolution or refresh rate; please keep the formula pixel clock = resolution x refresh rate in mind.  With a fixed hardware clock of 27 MHz, as you change your resolution (includes blanking), the refresh rate will be affected as well.  You can always play with the horizontal and blanking areas to achieve a visual resolution (valid video area) at a desired refresh rate as long as your display knows how to handle the blanking areas correctly.  This pixel clock, resolution, and refresh rate relationship is key.

    Aside from the above, when you change resolution, you need to change
    - driver level registers defining video frame (new resolution, including blanking areas)
    - application level buffer management to account for new buffer sizes
    - application level calls to any encoding/decoding codec to provide it the correct video resolution.I hope this helps!

     

    DM355 Appro
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • JamesS
    Posted by JamesS
    on Jul 27 2008 21:47 PM
    Prodigy190 points

    Appro has deviated a little from what software was delivered with our DVEM.  They have their own AEW library, that remains closed source, and TI have added the kernel source for this micron sensor.  They use and specify standard TI dvsdk_1_30_00_40.

    I am aware that the hardware from Appro won't do the required frame rates we are after.  Thanks for pointing out the formula.  Thanks for the tips on what needs to change to support various resolutions.

    Is there a single document that shows the flow of data through the system, from application right through to a sensor, and back again, for example?  I have found bits of information, but nothing that really ties it all together.  I've found the whole thing very frustrating so far.  I realise it is quite complex, but surely a breakdown from top level components into smaller parts would lay the whole thing out and make the task of comprehending how things fit and cooperate would be feasible. 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Juan Gonzales
    Posted by Juan Gonzales
    on Jul 28 2008 07:54 AM
    Mastermind33965 points

    I agree this can be quite complex.  Like most complex software architectures, there are various defined APIs (V4L2 driver, FBDev driver, codec engine...) which applications use to make all the various software components function together.  In my opinion, the key is to understand these APIs as well as where they fit in the software architecture (kernel space, user space,...).

    There are App Notes which describe this from the point of view of the demos provided in the DVSDK; for example http://focus.ti.com/lit/an/spraah0a/spraah0a.pdf

    As far as APIs go, Please keep in mind that most of the driver APIs are defined by Linux standards and hence we do not provide documentation for those (not defined by TI), but there should be plenty of documentation and example application online.  We do provide documentation for non-standard Linux drivers defined by TI and our codec engine APIs. 

    DM355 software architecture APIs
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use