Dear All,
I want to make a SD BOOT CARD on DM368 Board.
The SDK Version is dvsdk_4_02_00_06.
I followed the documention /dvsdk_4_02_00_06/psp/u-boot-2010.12-rc2-psp03.01.01.39/tools/uflash\README , and run the command as below:
root@avst-develop:/home/hunter/dvsdk_4_02_00_06/psp/u-boot-2010.12-rc2-psp03.01.01.39/tools/uflash# fdisk /dev/sdb1
WARNING: DOS-compatible mode is deprecated. It's strongly recommended to
switch off the mode (command 'c') and change display units to
sectors (command 'u').
Command (m for help): d
Partition number (1-4): 1
Command (m for help): n
Command action
e extended
p primary partition (1-4)
p
Selected partition 1
First cylinder (1-2160, default 1): 20
Last cylinder, +cylinders or +size{K,M,G} (20-2160, default 2160):
Using default value 2160
Command (m for help): w
The partition table has been altered!
Calling ioctl() to re-read partition table.
WARNING: Re-reading the partition table failed with error 22: Invalid argument.
The kernel still uses the old table. The new table will be used at
the next reboot or after you run partprobe(8) or kpartx(8)
Syncing disks.
root@avst-develop:/home/hunter/dvsdk_4_02_00_06/psp/u-boot-2010.12-rc2-psp03.01.01.39/tools/uflash# partprobe
root@avst-develop:/home/hunter/dvsdk_4_02_00_06/psp/u-boot-2010.12-rc2-psp03.01.01.39/tools/uflash# ./uflash -d /dev/sdb1 -u UBL.bin -b u-boot.bin -vv
UBL Size 20991
U-Boot Size 310391
First partition starts at 66500(34048000)
Required Blocks 774, Available Blocks 66499
UBL Magic Number : a1aced00
UBL Entry Point : 00000100
UBL Number of Blocks : 00000028
UBL Starting Block : 00000075
UBL Load Address : 00000000
Writing UBL Signature
Writing UBL
U-Boot Magic Number : a1aced66
U-Boot Entry Point : 81080000
U-Boot Number of Blocks : 0000025f
U-Boot Starting Block : 000000a7
Load U-Boot Address : 81080000
Writing U-Boot Signature
Writing U-Boot
Done...
The UBL.bin is UBL_DM36x_SDMMC_ARM432_DDR340_OSC24.bin from \dvsdk_4_02_00_06\psp\board_utilities\ccs\dm365.
The u-boot.bin is from \dvsdk_4_02_00_06\psp\u-boot-2010.12-rc2-psp03.01.01.39.
And I configure the switch to SD BOOT Mode. Insert the SD card to dm368 board, and power on.
In my opition, I will see the UBL and uboot logs from serial port. But I get nothing.Why? Is there some steps get error ?