Dear sir,
I am using IPNC camera with dm355 with the kernel version of 2.6.10.It was working fine suddenly it is not working it showing the kernel panic error as i shown in the below.
So I freshly loaded kernel and ramdisk form ti directly into the ram and try to boot instead of taking form nand flash then also it showing the same error sir.Filename 'uImage_ipnc_2.5.0'.