Hello,

In our application we are using DM365 with TLK110.
The ethernet 100Mbps connection is working without problem but we are getting problems with 10Mbps.

We are testing by connecting our Custom board to a 10Base-T Hub.

The SPEED Indication LED on both the board and Hub is OFF, so we can assume the link speed is detected as 10Mbps,
but the HUB doesn't detect the link up.

Meanwhile, we have checked the same with DM365 EVM and it works fine with
both 100Mbps/10Mbps connection.

Our circuit is almost same to the EVM reference schematics,
the only difference is we are using TLK110 PHY instead of Micrel.

Please let us know if there is troubleshooting tips in this issue
or any things to be considered in case of TLK110.


Best Regards