Hello,
I am trying to load uboot, ubl, uImage, squashfs using SD card.
Its explained very clearly in document USER_Guide_IPNC_DM36x under section 2.2.2
and also on
http://wiki.davincidsp.com/index.php/SD_card_boot_and_flashing_tool_for_DM355_and_DM365
I did following steps
1) Extract file dm3xx_sd_boot-6.1.zip located at Utils\src folder
2) Copy all the files reuiqred for burning like filesystem, uimage, uboot, ubl and diagnostic file to original folder
3) Edit dm3xx_sd.config and Makefile to choose the platform (DM36X or DM35X) and the modelname (DM365_IPNC or DM368_IPNC). Also set the mount path correctly as data_file=`<PATH where SD Card is mounted>/dm3xx.dat`
4) Now, Prepare the SD card, Insert a SD card ( SDHC is not supported) to a Linux PC
5) Find out the device name of this SD card by looking at /dev/sd*
6) Navigate to folder where dm3xx_sd_boot-6.1 is installed.
7) Run this command export PATH=$PATH:./bin.x86
8) User need run make command
Here make was successful
after that
9) Run command
sudo ./dm3xx_sd_boot format /dev/sdb (sdb is device name for SD card I used)
But in this step I am getting error
sudo: ./dm3xx_sd_boot: command not found
Kindly suggest solution for this issue