• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » DaVinci™ Video Processors » DM3x DaVinci Video Processor Forum » DM355 Rev A support for MT29F2G08ABAEAWP NAND
Share
DaVinci™ Video Processors
  • Forums
  • Announcements
Options
  • Subscribe via RSS

DM355 Rev A support for MT29F2G08ABAEAWP NAND

DM355 Rev A support for MT29F2G08ABAEAWP NAND

This question is not answered
Frank Hunleth
Posted by Frank Hunleth
on Aug 11 2012 18:32 PM
Prodigy90 points

I am trying to find out whether the DM355 Rev A will support MT29F2G08ABAEAWP NAND. This product had previously used a MT29F2G08AADWP NAND Flash part, but that part is no longer available. I am currently unable to get the product to boot with the new part, but I am unsure why it does not boot. The Micron TN-29-52 migration guide indicates that the parts have the following differences:

  1. Requires 4-bit ECC instead of 1-bit ECC
  2. Requires a reset command be sent on power up
  3. Has a different Manufacturer ID. (The device Flash ID is still 0xDA)
The reset command requirement concerns me since I cannot tell from the DM355 specification whether RBL 1.1 sends this command. I do not believe that the other two changes are preventing UBL from being loaded and run. We have tried manually programming the new NAND part with an external programmer and by running a program on the DM355 to burn it (booted via UART) with no success.
Two questions: First, is it known whether the MT29F2G08AADWP part works with a DM355 Rev A? If it won't work, are there any options that don't involve respinning the PCB?
Thanks,
Frank 
dm355 nand
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Renjith Thomas
    Posted by Renjith Thomas
    on Aug 12 2012 08:49 AM
    Guru23890 points

    Frank,

    I think the device should work without any issues. I have checked both the datasheets.

    1. 4-bit ecc can be supported in both devices (64 bytes spare area).

    2. The reset command (0xFF) is required for the MT29F2G08AADWP also.

    3. The manufacturer ID is same for both the devices. 0x2C. Only device ID is different, which shouldn't be a problem.

    How did you flash the NAND using external programmer? Is it using the same ECC algorithm that the bootrom needs? Is your programmer able to do a write and read back properly?

    Have you tried using the CCS application NANDWriter for flashing the image?

    -Renjith | www.pathpartnertech.com | Verify the answer if you think your query is resolved

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Frank Hunleth
    Posted by Frank Hunleth
    on Aug 12 2012 12:05 PM
    Prodigy90 points

    Thanks for the quick response. I had thought that the device should work too.

    Regarding the device ID, they both should be 0xDA according to the datasheet, right? I agree that I don't think that this is a problem, though, since 0xDA is in the RBL's supported device table.

    For the external programmer, the exact same ECC was used as before. No changes were made, but I can always double check.

    I am using the commandline utility sfh_DM35x.exe to program the Flash via the UART. I've tried a couple boards with the new Flash. The sfh_DM35x utility completes successfully for both like normal, but neither board shows the UBL or u-boot messages via the UART when they boot. If the new Flash part is unsoldered and an old Flash part put in its place, everything works perfectly.

    The only change is the Flash part. I made no changes to any other part of the programming process or anything else. If I need to change something, then that's my probably my issue, but I don't see anything to change. I'm at a loss as to why the new Flash part doesn't work, but I don't believe that it is due to a flaw in the programming process since I have been rechecking everything with the old Flash part. I've also tried multiple new parts.

    Could there be an issue with the DM355 Rev A that's causing the problem? This board uses the old version so we still have to use the legacy ECC layout.

    Thanks,
    Frank 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Renjith Thomas
    Posted by Renjith Thomas
    on Aug 12 2012 12:37 PM
    Guru23890 points

    Frank,

    There is one more thing. Have you checked the internal ECC support in the new NAND? You have to disable the internal ECC while writing and booting. I'm not sure whether internal ECC is enabled by default. 

    Another point to note is that ONFI support will not work if internal ECC is enabled. You can check both of these points. 

    What I'll suggest is to use the NANDwriter.out CCS tool to flash the binaries. You can get the source code for the same. You can also verify the data by modifying the code to read back and verify the contents. This will give you greater flexibility in debugging.

    -Renjith | www.pathpartnertech.com | Verify the answer if you think your query is resolved

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Frank Hunleth
    Posted by Frank Hunleth
    on Aug 15 2012 08:29 AM
    Prodigy90 points

    Renjith,

    We finally were able to make sure that internal ECC support was disabled with the external programmer. We're still seeing the same result. The Flash appears to program successfully, but the DM355 still will not boot from it. As far as we can tell, the Flash contents are exactly the same between the new and old Flash parts.

    Do you have any other ideas? I'm still worried that this may be a Rev A issue. Could you check on whether something could have been fixed between Rev A and whatever the latest DM355 revision is?

    Thanks,
    Frank 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Renjith Thomas
    Posted by Renjith Thomas
    on Aug 15 2012 14:54 PM
    Guru23890 points

    I am not sure about the Rev A and newer version difference. It could be possible. 

    How did you disable ECC support using external programmer? Is it done by sending SET_FEATURE command? If so, can you check whether this feature is set by default? Then there is a possibility that this is enabled during bootup and which can be cause the failure. Can you try reading back the data of the page-0 and see what are the values in spare area? Can you compare the same with the page-0 of the older NAND?

    If you have an oscilloscope or logic analyzer, can you try to see how many pages of data does the BOOT ROM reads? If its reading just one or max 4 pages, we can safely assume that there is some issue with the ECC logic itself.

    -Renjith | www.pathpartnertech.com | Verify the answer if you think your query is resolved

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use